Camera Selector

Vision China Shanghai 2024

Allied Vision, LMI Technologies, Chromasens, and SVS-Vistek will jointly participate in Vision China Shanghai 2024 at the TKH Vision booth. Visit us to explore the various vision solutions available from TKH Vision.

 

Booth number: Hall E1, 1402

8 - 10 July, Shanghai New International Expo Centre

Learn more 

 

Take your food sorting imaging task to the next level!

Alvium G1 cameras

DISCOVER MORE

AI-BLOX and Allied Vision

An exciting collaboration between AI-BLOX and Allied Vision. The modular edge technology platform called Blox will be integrating the new Alvium GM2 (GMSL2™ interface) cameras.

Read more

Last Time Buy for CCD cameras: August 31, 2024

Last-Time-Buy period for all Sony CCD-based sensors is ending soon. Place your order now!

Learn more!

Kudan and Allied Vision

A new exciting collaboration between Kudan and Allied Vision. The Kudan Grand SLAM software will now support the Nerian Ruby 3D depth camera and is available as part of Kudan’s Mobile Robot Development Kit for Autonomous Mobile Robots.

Learn more

High-resolution short-wave infrared cameras

Alvium SWIR cameras with Sony IMX992 and IMX993

Learn more 

Discover the Goldeye XSWIR Cameras

Goldeye XSWIR cameras with extended SWIR sensitivity up tp 2.2 µm and integrated dual-stage cooling (TEC2). 
Learn more about the award-winning Goldeye XSWIR cameras and XSWIR sensor technologies 


Find out more

Choose the right camera for your application

Go to camera selector

Take your career to the next level!

Allied Vision is looking for people like you. We are always on the lookout for ambitious professionals who share our passion for quality and innovation and who like to make our customers happy.

Find out more

Focus on what counts

We don't just develop cameras. We provide answers.

At Allied Vision, we help people achieve their goals with digital cameras for computer vision. This technology opens up a range of new possibilities for businesses throughout a broad spectrum of industries. Originally built with the needs of manufacturers in mind, our camera portfolio now extends to a wide variety of sectors including science and research, medical imaging, traffic monitoring, and sports analytics.

Given the wide variety of application challenges our customers face, we have always endeavored to offer a flexible and variable camera portfolio. This is why we design our cameras to be modular. The result is a diversity of sensors, lens mounts, filters, board-level versions, and many more options that maximize flexibility.

Discover more about Allied Vision

The image you need

Camera technology for your requirements

Our engineers design digital cameras with a large scope of resolutions, frame rates, bandwidths, interfaces, spectral sensitivities, sensor technologies, and technical platforms. We have created a modular concept to ensure that your camera adapts to requirements of your application and not the other way around.

We know how to help you find the best camera solution for your application. That includes a digital camera, but also the right lens, the right connectivity hardware and the right software interface. Our job is to reliably deliver the image you need, when you need it and how you need it.

 

Learn more about our pRODUCTS

From embedded to scientific

Vision solutions for your application

Do you need help

Technical information and support

Allied Vision is at your side throughout the life cycle of your image-processing project. We are here to help you integrate your camera into your system, solve software issues and ensure your system performs as it should even years after you purchased your camera.

Our specialists provide expert advice, engineering, manufacturing and support for digital cameras, their peripherals and their integration into your machine vision system.

Get an overview of helpful information and downloads!

Stay tuned!

Latest news

The Changing Face of Vision

Product News

To understand the trends, challenges, and opportunities of embedded vision it is necessary to first clarify the concept of embedded vision.

In our understanding, embedded vision is the merger of two different worlds:

  • Embedded systems and
  • Computer vision

Embedded systems represent the corresponding embedded boards that come into use in compact systems. Typically, embedded systems are small, lightweight, and low-cost computing devices that can be embedded into a larger system – for example a car, a robot, a security terminal, or a vending machine. They can also be mobile or battery-powered, such as in a video doorbell or body camera.

Computer vision began as an experiment in artificial intelligence. The goal was to reconstruct the human visual system, ultimately applying visual perception for performing some analysis. This takes place with the aid of cameras, but also with algorithms that were developed for very diverse mathematical operations.

The rise of embedded vision
For several years now, there has been demand from the embedded system world for more and more powerful cameras and algorithms to run these on embedded boards – for example for applications such as facial recognition or deep learning. The concept of embedded vision came to be. The goal is the interpretation and explanation of images and videos within an embedded system.

When it comes to adding vision to an embedded system, the designer is confronted with several challenges, especially concerning the choice of the cameras themselves. The main question is, how much image processing can be executed in the camera, and how much on the embedded board? Cameras for the embedded field nowadays are known for not executing much image processing as they are not as rich in features as in the machine vision sector. They deliver a passable image to the embedded board. Further processing steps must be carried out on the embedded board, which burdens the CPU. This in turn means that there is less capacity for other processing tasks. And to choose a better performing board would raise the total cost of the system.

Another challenge is the question surrounding standard interfaces on the cameras. In this market, a lot of terms like USB, LVDS, MIPI CSI-2, or PCI Express are used. Here, the challenge consists in finding the right interface for the application and implementing it with as little effort as possible. In this case, USB counts among one of the most beloved interfaces in use. However, USB has one big disadvantage: packets have to be packed and unpacked when they are sent. The CPU on the embedded board is burdened with additional expense that would be necessary for other tasks. For this reason, developers began choosing the MIPI CSI-2 interface, which is now used in hundreds of millions of smartphones and tablets. With the MIPI CSI-2 interfaces the CPU load is reduced in comparison to USB by up to 30%. Moreover, CSI-2 is a uniform standard that is continually optimized by the MIPI Alliance and its members.

Will embedded vision replace machine vision?
Even though embedded vision is developing very rapidly and dynamically, the machine vision market will not be impacted in every application. PC-based systems have not outlived their usefulness. There are still a few basic differences that could make PC-based systems preferable for certain application cases. PCs have still the advantage that they are more powerful (e.g. CPU, GPU) than embedded boards, which make them to the preferred choice for more demanding algorithms or applications. Furthermore, they will still play an important role as we say “all-rounders” and take care of the overall performance of the whole system. Whereas embedded systems are designed for one single functionality or only a few functionalities. They are just a part of a whole system or application. The full embedded system with its embedded board is designed for the necessary performance and cost-optimization. In most cases, this leads to the situation that the embedded system cannot be upgraded e.g. with additional peripherals in the future or only combined with a high cost increase. Here especially, we find the strength of a PC-based system or machine vision system with its flexibility. On the other hand, the initial costs for an embedded system are much lower than a PC-based system. It is only a matter of time where more performance will be available in embedded boards. This will accelerate the transition from PC-based systems or the classic machine vision to embedded systems or embedded vision.

The future is bright
There are many similarities between computer vision, machine vision, and embedded vision.  However, evolving applications in both consumer and industrial markets make embedded vision an attractive market.  Requirements for embedded vision are generating new approaches to vision technology, from cameras to processors and software algorithms. Based on the effort applied by significant players in the semiconductor market, embedded vision has a bright future.