相机选型工具
在线咨询
点击或扫码咨询
(无需添加好友)

基于索尼CCD传感器相机的末次购买和末次发货期限

采用索尼 CCD 传感器项目的抉择困难:即刻转型还是持续坚守?

我们支持您针对自身项目寻找更好的应对方案。

了解更多

Kudan和Allied Vision

Kudan与Allied Vision的合作备受期待。Kudan Grand SLAM软件现已支持Nerian Ruby 3D深度相机,并随同Kudan自主移动机器人的移动机器人开发套件提供。

 

了解更多

高分辨率短波红外相机

即将发布:

搭载Sony IMX992/993传感器的Alvium短波红外相机

 

了解更多

Goldeye XSWIR LP 扩展型短波红外相机

Goldeye XSWIR 扩展型短波红外相机
像素尺寸低至 2.2 µm,集成 TEC2 双重冷却技术


了解更多

 

为您的应用选择合适的相机

 

前往相机选型工具

 

专注于您的需求

我们不止于开发相机,我们探求答案。

在Allied Vision,我们致力通过计算机视觉数码相机助力客户达成目标。这项技术为各行各业的企业机构开辟了一系列全新机遇。我们的相机产品最初基于制造商需求打造,现已扩展到各个领域,包括科学与研究、医学成像、交通监控和运动分析。

 

鉴于我们的客户面临着各种应用挑战,我们始终致力提供灵活多样的相机产品线。这也是我们采用模块化相机设计的原因所在。最终,我们提供了各式传感器、镜头接口、滤镜、主板型号选择以及更多其他选项,最大限度提高灵活性。

 

了解更多

“相”您所想

可精准满足您需求的相机技术

我们的工程师设计的数码相机提供了海量的分辨率、帧率、带宽、接口、光谱灵敏度、传感器技术和技术平台选项。我们为此打造了模块化概念,确保相机可灵活适应您的应用需求,而不对您的应用设限。

 

熟谙如何针对不同应用场景寻找最适宜的相机解决方案。这既包括了数码相机本身,也兼顾了适配的镜头连接硬件以及软件接口。我们的工作是在任何场合以直观的方式可靠地输出所需的图像。

 

 

了解我们的产品

从嵌入式应用到科研

面向您应用的视觉解决方案

应您所需

技术支持

在图像处理项目的全生命周期中,Allied Vision为您提供全程支持。我们可随时助您将相机集成至自有系统,解决软件相关问题,确保系统在购入相机的数年内仍能发挥一贯性能。

 

我们的专家将为数字相机及其外设,以及它们与您机器视觉系统的整合提供专业的建议、设计、制造和支持。

查看技术文档和下载

时刻关注最新信息!

最新资讯

Collaboration between Allied Vision and Avnet Silica strengthened

Company News

EMEA-wide partnership with Allied Vision expands Avnet Silica’s embedded vision solutions portfolio

Avnet Silica expands its embedded vision solutions portfolio through EMEA-wide partnership with Allied Vision. Their mainline driver for Alvium cameras has been integrated and accepted into the Linux kernel, simplifying the integration of Alvium cameras into Linux and ARM platforms.

More and more vision applications are emerging in the field of AI and IOT edge. Therefore, customers have an increased need for fully integrated Embedded Vision solutions. With this in mind, Allied Vision and AVNET Silica, an Avnet company (NASDAQ: AVT), have agreed to strengthen their collaboration. Avnet Silica will include Allied Vision into its linecard as an EMEA-wide franchise. The agreement provides customers with complementary support for varied needs, from optics over cameras to image processing on embedded SoCs, through Avnet Silica’s EMEA Software and Services team.

Optimal compatibility with current and future embedded vision solutions
With its unique modular design, the Alvium platform offers a wide range of interfaces such as MIPI CSI-2 and GMSL2™, sensors, spectral sensitivities, resolutions, housing and mounting options as well as a driver API. For nearly every customer requirement for applications in the fields of Industrial Automation, Medical engineering, Logistics, Robotics and Food & Beverage, the appropriate integrated embedded vision solution can be developed quickly and easily now. It enables Avnet Silica customers to leverage short lead times and swiftly meet market demands, offering a variety of image sensors.

Avnet Silica Software and Services EMEA’s mainline driver for Alvium cameras has been integrated and accepted into the Linux kernel. "The availability of the mainline driver for the Alvium platform marks an extremely important milestone, not only for the cooperation between Allied Vision and AVNET, but also for the users. This driver ensures optimal compatibility with current and future embedded vision solutions and simplifies the integration of Alvium cameras into Linux and ARM platforms," says Torben Maschmann, Director, Software & Quality Assurance al Allied Vision, emphasizing the importance of this development.

Avnet Silica has already presented demonstrations of Allied Vision’s GMSL2 Alvium camera on Windows 10 IoT and an NXP i.MX8MPlus running mainline Linux at embedded world 2024 in Nuremberg. Visitors were able to discover the benefits of Avnet Silica and Allied Vision’s collaboration by attending a series of seminars which focus on the selection of cameras and module-based prototyping with Allied Vision and Avnet Embedded module solutions:

  • A modular Prototyping Approach for Embedded Vision Projects
  • Choosing the optimal Embedded Camera Solution for your Project